{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

What is the maximum number of buffered events allowed in a SCADAPack x70 RTU (DNP3 and IEC-60870-5-104)?

In legacy SCADAPacks (SP32/Sp3xx) the maximum number of DNP3 events was ~20,000. This was SCADAPack programmed with Telepace or SCADAPack Workbench CAM3 firmware. The legacy SCADAPack E (3xxE 53xE) could retain ~40,000.

If a end user is using a SCADAPack x70 RTU AND firmware 9.8.6 or greater, the maximum buffered events can be configured for DNP3 and IEC-60870-5 104 are set at 100,000 events. The default is set to 5000 events. This is configured on the events tab in RemoteConnect.

Max Events

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: