{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

What is the correct RBC for the SMT 2.2kVA and 3kVA rack-mount UPS Models?

Question: What is the correct RBC for the SMT 2.2kVA and 3kVA rack-mount UPS models?

Product Line: SMT2200RMI2UC, SMT2200RM2UC, SMT3000RMI2UC, SMT3000RM2UC

Environment: UPS units with ID 1027

Cause:  SMT 2.2kVA and 3kVA rack-mount UPS models with ID1046 may display the incorrect RBC model number on the UPS LCD Display, or the SmartConnect user interface. This will be addressed in an upcoming UPS firmware update.

Resolution: The correct RBC model numbers are shown below and on the UPS product pages on www.apc.com.
UPS ModelRBC
SMT2200RMI2UCRBC43
SMT2200RM2UCRBC43
SMT3000RMI2UCRBC43
SMT3000RM2UCRBC43

For more information on updating the firmware of your UPS, refer to Knowledge Base Article FA164737.

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: