{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
How to update M580 CPU NTP time via BMENOC0321 module
It is possible to update the cpu time from the NTP time provided by the BMENOC0321 MODule installed on the same rack. This is not done automatically, and we need to program It:

1- Enable the "Network Time Service" on the DTM of the BMENOC0321:

BMENOC0321 DTM

2- Open the "Network Time Service " in the service list and put the NTP remote server IP address. You can customise the Polling period, the Time Zone option, etc:


Network Time Service configuration

3- Import the attached program section in your program:

Import section

4- Configure the DFB by putting the module rack position and its IP address:

DFB configuration

5- Use the "Enable" pin to activate the DFB and the Sync_PLC to enable the time synchronization.

6- Enable "Dynamic Arrays" variables in the project settings:

Project settings

The CPU time will be updated after enabling the DFB:

Animated DFB

PS: No need to enable the "NTP client" service of the CPU.

Schneider Electric Global

Attachment(s)
NTP_NOC0321.7z [1.82 KB]
Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: