{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
Can a Model 6 MCC be configured to 415VAC 50Hz voltage system?

415v 50hz is available for Model 6 MCC's as a special. We can issue special pricing for the application. Will have to know if there are any control power transformers or power supplies that will need to be converted.

Schneider Electric Global