{}

Impact-Company-Logo-English Black-01-177x54
Share Price 
Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs

Smart-UPS Ultra 5kW Reports "0xC3E1" Alarm

Issue: The UPS reports "Event Code 0xC3E1" alarm on the LCD.
Note: this may lead to additional alarms being reported e.g., Battery Module Not Connected, Battery Disconnected

1 2 3

Product Line: SRTL5KRM2UI, SRTL5KRM2UT

Environment: UPS firmware version 03.1 or earlier

Resolution: This issue is addressed in UPS firmware version 03.2 Upgrade the UPS firmware to version 03.2 or later. Refer to FA170679 or FAQ000242942 for more information on how to update the UPS firmware.

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: