Search FAQs
Firmware / Hardware compatibility for Lexium 62 devices
Definitions:
Lexium 62 Standard
Lexium 62 Standard Plus: Successor device for LXM62 Standard with additional features
Lexium 62 Advanced Plus: New device based on LXM62 Standard Plus with additional features
The Lexium 62 Standard and the Lexium 62 Standard Plus have the same commercial reference, however, they can be distinguished by the revision number and the QR code on the front cover.
Hardware/firmware compatibility list:
*The new functions can only be used from FW V01.60.xx.xx onwards.
Lexium 62 Standard
Lexium 62 Standard Plus: Successor device for LXM62 Standard with additional features
Lexium 62 Advanced Plus: New device based on LXM62 Standard Plus with additional features
The Lexium 62 Standard and the Lexium 62 Standard Plus have the same commercial reference, however, they can be distinguished by the revision number and the QR code on the front cover.
Hardware/firmware compatibility list:
Device type | Commercial Reference | HW Revision | QR code on the front of the device | Compatible firmware |
Lexium 62 Standard | LXM62DxxxC LXM62DxxxD | RS0x | No | V01.32.xx.xx - V01.54.xx.xx |
Lexium 62 Standard Safety | LXM62DxxxE LXM62DxxxF | RS0x | No | V01.54.xx.xx |
Lexium 62 Power Supply Standard | LXM62P | RS0x | No | V01.32.xx.xx - V01.54.xx.xx |
Lexium 62 Standard Plus | LXM62DxxxC LXM62DxxxD | RS1x and higher | Yes | V01.36.12.xx - current FW * |
Lexium 62 Standard Plus Safety | LXM62DxxxE LXM62DxxxF | RS1x and higher | V01.54.xx.xx – current FW * | |
Lexium 62 Advanced Plus | LXM62DxxxG | RS1x and higher | Yes | V0.1.60.xx.xx - current FW |
Lexium 62 Advanced Plus Safety | LXM62DxxxH | RS1x and higher | V01.60.01.xx – current FW | |
Lexium 62 Power Supply Standard Plus | LXM62P | RS1x and higher | Yes | V01.36.12.xx – V01.54.xx.xx |
Released for:Schneider Electric Global
Explore more
Range:
Explore more
Range: