Search FAQs
How to read and modify variable by sending SMS to the Zelio Smart Module?
- In ZelioSoft:
Regarding the Parameters, select people who are authorized to send Modification command and define the variable access to “Read and modification”:
- Connection to the Zelio Smart module:
From this window, define the access key which will be used in the command to read/modify variable(s). By default, it is 00000000.
- On Mobile phone:
To modify the value of the variable which has the Alias B003, send the following command via SMS: 00000000!B003=1
(In that case, the value '1' will be written in the variable having the Alias B003)
If the variable and/or the recipient only have the read access, the following error should appear when trying to modify the value:
Released for:Schneider Electric Global
Explore more
Product:
Range:
Explore more
Product:
Range: