{}

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric corporate Website

Search FAQs
What is the storage recharge guidelines for the SRYLBM?

Product Line:

SRYLBM


Environment:

Smart UPS Modular Ultra, Smart UPS Ultra 5kva, 8kva and 10kva


Resolution:

Storage limits

Maximum storage time without recharge

Temperature

-15 to 35 degrees C (5 to 95 degrees F)

9 months

35 to 45 degrees C (95 to 113 degrees F)

6 months

Elevation

0 - 15,000 m (0 - 50,000 ft)

Humidity

0% to 95% relative humidity, non-condensing

NOTE:

  • Charge the battery modules as soon after receipt as possible.
  • Ambient storage temperatures above 25°C will shorten battery life.

Schneider Electric Global