1. Two wire control means, two wires for drive start command of "Forward and Reverse". In two wire control there is no separate stop command is provided. The forward and reverse command is...
Issue: Where can we find the download links for Vijeo Designer V6.2 SP12? Product Line: Vijeo Designer V6.2 (all hotfixes and service pack revisions less than SP12) Resolution: Please find the...
Issue Register list for Modbus communication Product Line PM5110, PM5330, PM5340, PM5560, and PM5563 Environment Power Meter Communications Modbus Register List Cause PM5000 series register list is...
Issue: Connecting SoMove to the VFD using the Ethernet network connection. Product Line: ATV61 ATV71 ATV630 ATV930 ATV320 ATV340 ATV32 ATV320 Environment: Ethernet IP or Profinet option installed....
Issue: Freewheel stop assignment on ATV61/71. Product Line: Altivar 61 and 71 Environment: All models and serial numbers Cause: None Resolution: Go to Drive menu, 1.7 Application function menu, and...
It is possible in Oil Distribution Transformers, but can only be done by an authorised service. Please consult to Schneider since unauthorised attempt will cause warranty loss.
Drivers Windows 7 for iDisplay iDisplay Touch screen drivers for W 7 32 and 64 bits Goals and Symptoms Currently, our iDisplays are supplied only with the Windows XP drivers for Touch screen. The...
PUP is the "pick-up" of the fault. Often people mistake "PUP" as the pickup of disturbance recording, but this is incorrect because the disturbance recording is often configured...
AC-3e rating is the capability of the contactor for starting and switching off high efficiency squirrel cage asynchronous (IE-3/ IE-4) motors during running and reversing operations, which have...
In PLC side: 1.Use TIA Portal V11-V16 to configure the PLC communication settings. 2.Select the PLC and enter the correct version of the firmware (We can check for the firmware version of the PLC in...
As there is an impedance mismatch at the termination of the motor cable to the motor, there will be a reflected wave which travels back along the motor cable causing overvoltage’s. Overvoltage’s on...
Issue: What is Power Factor Correction (PFC) - Does it help conserve energy? Answer: Explanation 1: Power Factor Correction (PFC) doesn't directly reduce the overall electric consumption of a...
The 3rd party validated (Type III) PEP according to ISO 14025 provides transparent, comparable and reliable environmental data on product level, e.g on carbon footprint (CO2 eq). Standardized...
Please refer to the setting in the following picture: The setting gives you the option to turn system error window on or off. Select Yes to show system error message window on the panel at runtime....
Question : How to change the Cipher Suites of an NMC3 Product Line / Environment : Network Management Card 3 – AP9640/AP9641/ AP9643 and/or Devices with an embedded Network Management Card 3 Answer :...
Configure MTZ breaker accessories(MX1,XF,MN,MX2,MCH,M2C,ESM,RAR,BPFE) in EcoStruxure Power Commission will help customer to manage the breaker efficiently, find attached detailed procedure.

Support Center
Download Center
1. Two wire control means, two wires for drive start command of "Forward and Reverse". In two wire control there is no separate stop command is provided. The forward and reverse command is given through switch, so if the run command is high - the drive will run. If the run command is removed - the...
Issue: Where can we find the download links for Vijeo Designer V6.2 SP12? Product Line: Vijeo Designer V6.2 (all hotfixes and service pack revisions less than SP12) Resolution: Please find the download links for Vijeo Designer V6.2 SP12 below. Please download the zip file and extract it to get the...
Issue Register list for Modbus communication Product Line PM5110, PM5330, PM5340, PM5560, and PM5563 Environment Power Meter Communications Modbus Register List Cause PM5000 series register list is needed for Modbus communication Resolution See the attached documents for Register List.
Issue: Connecting SoMove to the VFD using the Ethernet network connection. Product Line: ATV61 ATV71 ATV630 ATV930 ATV320 ATV340 ATV32 ATV320 Environment: Ethernet IP or Profinet option installed. VW3A3316, VW3A3320, VW3A3627 VW3A3720 Cause: Drive is not detected when attempting to connect....
Issue: Freewheel stop assignment on ATV61/71. Product Line: Altivar 61 and 71 Environment: All models and serial numbers Cause: None Resolution: Go to Drive menu, 1.7 Application function menu, and assign Freewheel Stop assignment to a logic input (LIx) as desired. NO. MENU...
It is possible in Oil Distribution Transformers, but can only be done by an authorised service. Please consult to Schneider since unauthorised attempt will cause warranty loss.
Drivers Windows 7 for iDisplay iDisplay Touch screen drivers for W 7 32 and 64 bits Goals and Symptoms Currently, our iDisplays are supplied only with the Windows XP drivers for Touch screen. The gola of this resolution is to provide the drivers W 7 32 and 64 bits. Causes and Fixes The news drivers...
PUP is the "pick-up" of the fault. Often people mistake "PUP" as the pickup of disturbance recording, but this is incorrect because the disturbance recording is often configured with pre-trig cycles that are used to view the recording before the actual disturbance. "PUP" relates to the...
AC-3e rating is the capability of the contactor for starting and switching off high efficiency squirrel cage asynchronous (IE-3/ IE-4) motors during running and reversing operations, which have extended/ higher locked rotor current.
In PLC side: 1.Use TIA Portal V11-V16 to configure the PLC communication settings. 2.Select the PLC and enter the correct version of the firmware (We can check for the firmware version of the PLC in online mode). 3.Check the PLC firmware version in online mode, make sure the firmware version is...
As there is an impedance mismatch at the termination of the motor cable to the motor, there will be a reflected wave which travels back along the motor cable causing overvoltage’s. Overvoltage’s on the motor terminals can cause both partial and corona discharge which eventually wears down the...
Issue: What is Power Factor Correction (PFC) - Does it help conserve energy? Answer: Explanation 1: Power Factor Correction (PFC) doesn't directly reduce the overall electric consumption of a device or system, but it does play a role in optimizing the efficiency of electrical systems, which can...
The 3rd party validated (Type III) PEP according to ISO 14025 provides transparent, comparable and reliable environmental data on product level, e.g on carbon footprint (CO2 eq). Standardized environmental product data is provided from the PEP in all lifecycle stages based on a Life Cycle...
Please refer to the setting in the following picture: The setting gives you the option to turn system error window on or off. Select Yes to show system error message window on the panel at runtime. If you select No, the panel will hide the window. This property does not affect the generation or...
Question : How to change the Cipher Suites of an NMC3 Product Line / Environment : Network Management Card 3 – AP9640/AP9641/ AP9643 and/or Devices with an embedded Network Management Card 3 Answer : Users may need to adjust the list of SSL/TLS ciphers in use for NMC web access on the NMC,...
Configure MTZ breaker accessories(MX1,XF,MN,MX2,MCH,M2C,ESM,RAR,BPFE) in EcoStruxure Power Commission will help customer to manage the breaker efficiently, find attached detailed procedure.