The case for BESS
Steven Carlini
26 Jun 2025 • 4 min
The lights can never go out in a data center — until they do. And traditional backup systems weren’t built for climate change in the 21st century.
Overview
The data center industry is grappling with a trio of challenges that threaten to upend decades of established practice. Artificial Intelligence workloads are devouring electricity at unprecedented rates, while increasingly volatile weather patterns and renewable energy integration strain an aging power grid beyond its limits.
This convergence creates a compelling case for Battery Energy Storage Systems (BESS) that transform data centers from passive consumers into active participants in the energy economy, and a new strategic component of modern data center operations.
Schneider Electric's Data Center Research & Strategy group identifies several critical market dynamics reshaping data center power requirements. The exponential growth of AI applications has amplified energy consumption patterns , while the accelerating transition to renewable energy sources—despite their sustainability benefits—introduces intermittency challenges that traditional backup systems cannot adequately address.
Battery Energy Storage Systems represent a fundamental evolution from conventional data center power architectures. Unlike Uninterruptible Power Supply (UPS) systems that provide five to 15 minutes of backup power, BESS typically store one to two hours of energy, enabling multiple operational benefits beyond emergency backup.
The technology operates as an electrochemical device that stores energy from the utility grid and supplies it back to the grid or connected loads when needed. This dual functionality positions BESS as both a solution to increase resilience and a strategic asset for data center providers to participate actively in the grid.
BESS that are deployed on site at data center facilities offer operators several distinct advantages:
01
Flexibility and resilience
Better operational continuity during grid outages or fluctuations through extended backup power duration.
02
Cost optimization
Peak shaving and load shifting capabilities to offset peak demand charges, which can account for between 30% and 70% of monthly electricity bills for commercial customers.
03
Sustainability leadership
Supporting carbon reduction goals while addressing increasing regulatory challenges.
The financial implications of BESS deployment extend beyond traditional cost-avoidance metrics. Demand charges, based on the highest power consumption during 15 or 30-minute intervals within a billing period, represent a significant operational expense that BESS can directly address through strategic discharge during peak periods.
Recent regulatory developments and tax incentive clarifications in many countries have further enhanced the economic proposition. Government programs may reduce BESS deployment costs while creating opportunities for data centers to monetize stored energy by providing grid services during utility peak load periods, potentially transforming energy infrastructure from a cost center to a revenue generator.
Despite the compelling value proposition, BESS deployment requires careful consideration of site-specific factors. The return on investment varies significantly based on load profiles, local market conditions, regulatory frameworks, and specific use cases. Organizations must address several strategic questions before implementation:
01
Strategic alignment
Integration requirements with long-term business objectives and sustainability commitments.
02
Cost-benefit analysis
Comprehensive financial modeling comparing BESS to conventional backup solutions, including upfront investment, operational expenses, and potential savings.
03
Regulatory compliance
Navigation of jurisdiction-specific deployment frameworks and permitting processes.
04
Risk management
Operational risk mitigation strategies for grid outages, energy price volatility, and environmental compliance.
As the energy landscape increasingly adopts renewables and the grid is further decentralized, data centers that proactively integrate BESS capabilities will be better positioned to navigate operational challenges while capitalizing on emerging market opportunities.
Latest in Electricity 4.0
Need help?
Start here!
Find answers now. Search for a solution on your own, or connect with one of our experts.
Contact Support
Reach out to our customer care team to receive more information, technical support, assistance with complaints and more.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Browse FAQ
Get answers you need by browsing topic-related Frequently Asked Questions (FAQ).
Contact Sales
Start your sales inquiry online and an expert will connect with you.