Select the layout that most closely matches the environment:
Ancillary IT Area
Row-based IT Load
Row-based IT & Cooling Area
Ratio of L to W
2
X
Row-based Equipment Configuration Details
Temperatures Units
°F
X
1000 kW
X
Type of Cooling Devices
RP chilled water 600mm
X
Quantity of Cooling Devices
16 (minimum)
X
IT Equipment Population
80%
X
1U-2U
10%
X
Blade
+
+
Other
10%
=
100%
Chilled Water Entering Temperature
Chilled Water ∆T
50 °F
X
9 °F
X
Results
Temperature & Capacity
Row-based IT temperature
Ancillary IT temperature
Ancillary IT load vs. excess cooling
71 °F
74 °F
Ancillary load
50 kW
Excess cooling
55 kW
PASS
PASS
PASS
Adjustable Parameters
Cooling Devices Set Point
70
70 °F
Maximum Row-based IT Temperature
81
81 °F
Maximum Ancillary IT Temperature
81
81 °F
Ancillary IT Floor Area
20%
Ancillary IT Load
50
50 kW
Summary
No additional cooling is necessary. The ancillary load of 50 kW raised the row-based IT temperature by 1 °F. This is about 10 °F below the maximum row-based temperature of 81 °F.