Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

A changing grid requires flexibility

 

By Dwibin Thomas, Cluster Automation Leader at Schneider Electric

30 January 2024

Winston Churchill said, "To improve is to change; to be perfect is to change often."  It is a wonderful sentiment that can be applied in almost all industries including power generation.  As the landscape changes so should energy production and distribution (readily) adapt, ensuring that we establish a flexible, optimised grid of the future.

Traditionally, grid flexibility involved utilities enrolling large industrial energy consumers in load curtailment and demand response (DR) programmes to help adjust the balance between supply and demand. These electro-intensive users would reduce or shift their energy use during peak periods.

However, today grid flexibility has become far more complex.  For one, an increasing investment in renewables means that energy flow is bi-directional, with decentralised energy coming from multiple DERs (distributed energy resources). 

Furthermore, as organisations and even individual households start moving over to generating their own electricity, we now have growing landscape of prosumers that both produce and consume energy, further amplifying the need for grid flexibility.

Traditional demand response shows its limitations in balancing an evolving grid. It represents a critical paradigm shift for utilities, and given the pace of innovation, it is challenging to plan for a future that includes rapidly growing DERs.

Plus, and this is a fundamental challenge, upgrading a decades-old grid takes time and represents large capital expenditures. Grid-connected prosumers, an increase in electrification, and climate uncertainty also mean energy demand will continue to be variable and uncertain.

Digitisation leads to flexibility

A digitised grid – one that adapts to these variable energy sources and responds to dynamic challenges – is needed to identify, enrol, and aggregate distributed energy resources. These grids of the future realise sustainability as it can incorporate DERs in a more flexible and optimised manner to grid resilience. It adapts faster and is more responsive to weather crises, are more sustainable, more reliable, and can reduce operational costs with predictive maintenance strategies.

Through digitisation, operators benefit from a consolidated view of the various energy resources that are feeding into the grid, ensuring that it is managed and distributed methodically, based on real-world demand and supply.

Receiving energy from various DERs without proper management is pointless. This lack of management could potentially lead to an overloaded infrastructure and compromised power quality.

Change requires flexibility

As mentioned, to establish a more flexible grid we’ll have to keep pace with an evolving landscape. For one, at the prosumer level we’re see a hybrid future taking shape. On one side, more IoT-connected assets (buildings, houses, EVs, and so on) are online, ready to be dispatched and aggregated.

These assets are looking for the right “flex” compromise between efficiency through more automation, and freedom of choice enabled by customer engagement platforms.

Second is the grid management, here utilities must optimise each hybrid prosumer and other suppliers of DERs by incorporating the necessary technology (directly or via services vendors) that will enable it to become more agile and flexible.

At the distribution system operator level, there are DER management software solutions available that are tailored to enable the efficient planning, design, and operation of today’s flexible, dynamic grid.

These solutions maximise the connection of renewables by leveraging DER flexibility at every level. This approach supports small proof-of-concept projects to full-scale deployment rollouts that require direct device monitoring, control, and integration with third-party aggregators.

DERs management solutions provide energy suppliers and distributors with smarter, more efficient ways to manage the integration of various energy sources into their grid.

At Schneider Electric, for example, our DERs management software options incorporate AI and machine learning (ML) algorithms, not only analysing historical data but also considering weather patterns and forecasts that will give utilities additional insight into the renewable energy supply.

Adoption of Wiztopic's Blockchain Certification Platform

From 2nd October 2019, in order to secure its communication, Schneider Electric has been certifying its content on Wiztrust. You can check the authenticity on the website Wiztrust.com for corporate communications.
View press release (pdf, 185 kb) opens in new window
Share this page:

Chat

Do you have questions or need assistance? We’re here to help!