Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.

Distributed Energy Resource Management Systems (DERMS) – managing the wondrous instruments that bring us the grid symphony

By Taru Madangombe, Vice President: Power and Grid for Middle East and Africa at Schneider Electric

02 October 2024

 

To listen to a symphony is one of the world’s great gifts.  The culmination of instruments, diverse yet so beautiful when brought together by a competent conductor.  That one individual that ensures rendition, cohesion, and harmony.

A Distributed Energy Resource Management System (DERMS) is the conductors of the grid symphony that is made up of an extremely valuable yet varied mix energy resources (read instruments) such as rooftop solar, battery storage and traditional fossil-based energy.

 

A conductor must ensure that instruments play beautifully as a whole and are kind to the ear and uplifting to the spirit yet shine in their individuality.  The same can be said of a DERMS, which must effectively manage diverse energy sources to avoid compromising the grid’s integrity.

And it’s not only energy resources, DERMSs also work hand in hand in coordination with various other grid technologies such as outage management systems and Supervisory Control and Data Acquisition (SCADA) systems. This integration is vital, especially at the distribution level, where a fully-fledged system is required to balance supply from distributed energy resources (DERs) such wind, solar PV, and battery storage, with the load demand.

The delicate load balance.

 

The load profile of a power grid typically peaks in the morning, afternoon, and evening. Here, DERMS ensure that energy from DERs is used efficiently, avoiding wastage. For example, when the load is low, DERMS can control the output from batteries and solar systems, preventing oversupply and overvoltage.

Looking closer at overvoltage, like its brownout sibling, it can cause damage to appliances and grid infrastructure.

For example, household appliances are typically rated for 230 volts. If the grid experiences an overvoltage, pushing the supply to 300 volts, these appliances could be damaged. Similarly, grid infrastructure like transformers and switchgear, rated for specific voltages, can be damaged by overvoltage, leading to power outages.

 

DERMS help manage and mitigate these risks, ensuring the grid remains within safe operational limits.

In addition to grid stability, DERMS also play a role in energy trading. Some countries are leveraging DERMS for real-time energy trading, allowing consumers to choose the type of power they consume. For instance, consumers can opt to use only green power during certain times of the day. This capability aligns with the concept of virtual power plants (VPPs), where a network of DERs forms a single grid that utilities can tap into during high demand or reserve for later use.

 

At Schneider Electric, our DERMS platform forms part of our EcoStruxure Advanced Distribution Management System (ADMS) which provides a comprehensive solution for managing and optimising DERs. EcoStruxure ADMS is an industry benchmark used by 75 utility companies that serve 70 million end customers around the world.

One of the key advantages of our DERMS is its modularity. The platform can be integrated into existing utility enterprise systems, offering flexibility and scalability. This enables utilities to implement DERMS as part of a broader ADMS or as a standalone solution, depending on their specific needs.

Adoption of Wiztrust's Blockchain Certification Platform

From 2nd October 2019, in order to secure its communication, Schneider Electric has been certifying its content on Wiztrust. You can check the authenticity on the website Wiztrust.com for corporate communications.
View press release (pdf, 185 kb) opens in new window
Share this page:

Chat

Do you have questions or need assistance? We’re here to help!
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.