Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Hotels of the future are built on interoperable solutions

16 August 2023

The hospitality industry has always been cut-throat; guests are spoilt for choice and as a result hotels, large and boutique have to keep pace to ensure they offer features that differentiate them from the competition.

Whilst traditional challenges such as energy cost, cleaning expenditure and customer loyalty continue to define the roadmap to hotel profitability, technology also has a major part to play in not only raking up those review stars but also optimising operations.

Technology investments should be focused not only on higher comfort and convenience standards but also solutions that allow hotels to run more efficiently, particularly in a time when energy provision remains a foreseeable challenge.

Looking at guest convenience and comfort, today’s premier hotels feature innovation such as using phones as virtual keys and host of room options such as the ability to launch live chats with front desk staff from their smartphones, “touchless” operation in-room entertainment, room service, and comfort control systems (i.e., lighting, temperature, and curtains).

The benefits are real

From hotel owners and operators’ perspective, technology innovation offers important benefits:

Improved guest well-being and comfort – guests will have access to several human-to-room interface options to increase their level of comfort. These room control solutions can be configured via an easy-to-download smartphone app.

Other solutions include flat wall-mounted touch panel interface screens with customised surfaces that make it easy for guests to experience contactless, remote hotel check-in/out, and room service and concierge capabilities.

Operational and energy efficiency improvement – room control solutions allow conditions to be adjusted automatically, based on pre-set parameters, when rooms are either in “occupied” or “unoccupied” status.

Schneider Electric’s EcoStruxure for Hotels Guest Room Management Solutions for example utilise occupancy-based energy management to adjust room conditions while guests are away, and quickly restore those settings as soon as they return.

When the guest room is unrented or unoccupied, temperature reverts either to setback mode (unoccupied) or deep setback mode (unrented). Curtains are closed to mitigate solar heat gain or loss and to preserve furnishings.

Underfloor heating, mirror heating, and lights are turned off. This energy management functionality drives deep energy savings and reduces carbon emissions.

Moreover, during off-peak times, occupancy can be allocated in certain parts of the hotel which for example, has seafront views whilst the rest of the hotel can remain unoccupied, using minimal energy until peak season kicks off.

Faster, more responsive maintenance – maintenance staff can remotely identify issues before entering a room and quickly address them with minimal disruption.

Predictive maintenance, via the use of local sensors and analysis software, provides early warning signs before in-room electrical or mechanical systems break down. This allows maintenance staff to come in during off-hours to perform needed maintenance.

The right solutions

When choosing a solution to improve occupancy and overall building management efficiency, it’s important that owners and operators consider the following technology solutions:

  • A connected room solution, optimised for hotels.  These systems feature a modular, IoT ecosystem that provides occupancy- based energy management and guest room control enabling guests to fully customise their in-room experience.
  • Guest room management software which in tandem with a connected room solution provides centralised visibility and control of guest rooms and other services like BMS (Building Management Systems), PMS (Property Management Systems), door lock, housekeeping and maintenance systems for remote troubleshooting, proactive maintenance, and optimised workflows.
  • Open-integration BMS that monitors, manages, and controls building operations all on one system. Built on open standards and end-to-end cybersecurity, it integrates and facilitates data exchange from connected room solution and guest room management software to improve productivity, reduce guest complaints, and enable superior operational efficiency and guest room functionality.

Adoption of Wiztopic's Blockchain Certification Platform

From 2nd October 2019, in order to secure its communication, Schneider Electric has been certifying its content on Wiztrust. You can check the authenticity on the website Wiztrust.com for corporate communications.
View press release (pdf, 185 kb) opens in new window
Share this page:

Chat

Do you have questions or need assistance? We’re here to help!