Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

New Schneider Electric Easy UPS 3-Phase Modular is at the Forefront of Reliability, Scalability, and Simplicity Modular design with Live Swap feature for small and medium size data centers and business-critical applications.

  • 3-Phase 50-250 kW (400V) modular UPS solution with 50 kW Live Swappable power and static switch modules
  • Offers best-in-class power protection and optimized capital investment
  • Provides scalability and redundancy in a compact footprint
  • Proves Schneider Electric’s sustainability leadership as part of its Green Premium programme

 

 

Schneider Electric, the global leader in the digital transformation of energy management and automation, introduces Easy UPS 3-Phase Modular. This robust uninterruptible power supply (UPS) is designed to protect critical loads while offering third-party verified Live Swap functionality. Easy UPS 3-Phase Modular available in 50-250 kW capacity with N+1 scalable configuration and supports the EcoStruxureTM architecture, which offers remote monitoring services.

With scalability top of mind, Easy UPS 3-Phase Modular enables you to pay as you grow, allowing you to optimize capital investment. It is a part of Schneider Electric’s Green Premium portfolio, which ensures energy efficiency, durability, recyclability, and transparency to help reduce environmental footprint. In addition, this system features advanced technology such as a high-efficiency design, intelligent battery management, real-time monitoring, and control capabilities, making it one of the most cost-effective and energy-efficient UPS solutions available in the market.

 

“We are excited to introduce Easy UPS 3-Phase Modular to the market,” said Mustafa Demirkol, VP of Offer Management and Marketing for Data Center Solutions. “This product provides customers with third-party certified Live Swap, modular design, and unwavering reliability in an optimized investment package. Its connectivity provides peace of mind, making it the easy choice for data centers and commercial and industrial applications.”

 

Business continuity made easy

Easy UPS 3-Phase Modular enables customers to lower their capital expenditures through an optimized capex model. In addition, scheduled downtime is significantly reduced through self-diagnosing third-party certified Live Swapable power modules and static switch, thereby increasing reliability and availability in a compact footprint. Easy UPS 3-Phase Modular is easy to select, configure, install, and maintain, which makes the deployment process seamless. Easy UPS 3-Phase Modular is part of Schneider Electric’s Easy UPS 3-phase product portfolio, which focuses on core features to meet the needs of customers at a value price point.

 

About Schneider Electric
Schneider’s purpose is to empower all to make the most of our energy and resources, bridging progress and sustainability for all. We call this Life Is On.

 

Our mission is to be your digital partner for Sustainability and Efficiency.

 

We drive digital transformation by integrating world-leading process and energy technologies, end-point to cloud connecting products, controls, software and services, across the entire lifecycle, enabling integrated company management, for homes, buildings, data centers, infrastructure and industries.

 

We are the most local of global companies. We are advocates of open standards and partnership ecosystems that are passionate about our shared Meaningful Purpose, Inclusive and Empowered values.

 

www.se.com

 

Adoption of Wiztopic's Blockchain Certification Platform

From 2nd October 2019, in order to secure its communication, Schneider Electric has been certifying its content on Wiztrust. You can check the authenticity on the website Wiztrust.com for corporate communications.
View press release (pdf, 185 kb) opens in new window
Share this page:

Chat

Do you have questions or need assistance? We’re here to help!