BlokSeT’s iPMCC (intelligent Power and Motor Control Centre) is an advanced smart solution that provides for fault prevention, protection, and automatic restart. New temperature and humidity monitoring thermal sensors incorporated into the iPMCC achieve significant improvements in safety and reliability. The permanent thermal monitoring system uses small plastic non-contact and non-powered IR sensors that extend the maintenance lifecycle and mitigate safety risks such as electrical fires.
In addition, ergonomic design improvements make the BlokSeT LV switchboard easier and safer to operate and maintain.
With EcoStruxure IoT-enabled solutions, switchboard data can be collected and analysed in real time via wireless connectivity, giving operators the information they need for predictive maintenance.
The next generation BlokSeT LV switchboards consolidate Schneider Electric’s dedication to maximising uptime and enhancing safety, reliability, and connectivity for industry professionals.
For more information visit: www.se.com
For more information, go to www.se.com/za/en/.