21 November 2023
In times of crisis, it's essential that the country explores a disruptive approach, said Taru Madangombe, Vice President: Power and Grid for Middle East and Africa at Schneider Electric.
Addressing delegates at the recent AMEU event, held in at the CSIR Convention Centre in Tshwane, Madangombe noted it is not only South Africa’s current energy crisis that is driving disruption but a multitude of industry related trends, from new utility revenue models, climatic impacts, cybersecurity risk, to the rise of energy prosumers and the proliferation of renewable energy sources.
“The overall electricity value chain (Generation, Transmission & Distribution) is like an orchestra and each new instrument, whether it’s a distributed energy resource or prosumer, requires the reimaging of a well-known symphony to ensure the music remains harmonious and recognisable, and thus the smart GRID becomes the conductor or master of this orchestra” said Madangombe.
Playing an important role in ensuring harmonious grid operations is digitisation, which is rapidly becoming the driving force behind the evolution of the energy landscape. "We need to consider the entire energy value chain, from energy efficiency measures within homes to innovative grid solutions. Technology, particularly coupled with software digitisation, is key to creating a more energy-conscious and flexible energy infrastructure,” he explained.
Utilising digitisation as part of the recomposed energy landscape offers the following benefits:
- Grid management - digital technologies enable smarter grid management. Grids equipped with sensors and communication systems can detect issues, adapt to changes in demand, and optimise the flow of energy. This enhances grid reliability and resilience.
- Enhanced energy efficiency - through real-time monitoring and data analytics, energy systems can be optimised for maximum efficiency.
- Predictive analytics and forecasting help grid operators manage the intermittency of renewable energy, ensuring a stable energy supply.
- The decentralisation of energy generation. Small-scale renewable energy installations, such as rooftop solar panels, can be integrated into the grid with ease. This democratises energy production and reduces reliance on centralized power plants.
- It plays a role in extending access to energy in remote or underserved areas. Microgrids and off-grid solutions that incorporate digital technologies can provide reliable energy sources to communities that were previously off the grid.
Concludes Madangombe: “The energy trilemma is even more unique in the African context, as reliability, sustainability, and affordability are significant challenges. To overcome these, we must look at energy efficiency, electrification, and digitisation as a combined solution.
“And whilst technology alone is not enough; we need to create an enabling environment for all players. Digitisation may not be the only solution, but it's the best choice for the energy transition, helping us find the right balance between supply and demand while enabling monitoring and control,” concluded Madangombe.