Designed according to IEC 60947-6-1, TransferPacT is a PC class ATSE available from 32A–160A, 2,3,4 pole with a rated operating voltage of 220V–440V.
The TransferPacT product family comes in two different offerings: Automatic and Active Automatic. TransferPacT Automatic provides quick settings and an easily viewed interface. TransferPacT Active Automatic offers a more comprehensive functionality, with a built-in controller and display, and the option to extend to an external HMI.
The scalability that TransferPacT provides enables a user to extend a source changeover solution so that further transfer switch modules can be added as demand grows and upgrades can be scheduled without any interruption of power.
TransferPacT ATSE features include increased power availability and efficiency boosted by connectivity and cybersecurity. Uptime is maximized with innovative technology that ensures transfer speeds of < 500ms. A compact and robust design helps TransferPacT perform in the harshest environments, with operating temperatures of -25°C through to 70°C. A built-in DPS and sensing wire means users enjoy a 30% time saving on installation and commissioning.
EcoStruxure IoT-enabled solutions collects and analyses ATSE data in real-time via wireless connectivity giving operators proactive – rather than preventive – maintenance analysis.
Given its robust and reliable performance that maintains power continuity and sustainability, TransferPacT ATSE has been specifically designed to boost the buildings sector, healthcare facilities, data centres, and transportation.
With the next generation TransferPacT ATSE product family, Schneider Electric further establishes its dedication to maximising uptime and enhancing safety, reliability, and connectivity for industry professionals.