Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.

Schneider Electric’s SpaceLogic Living Space PM sensors redefine indoor air quality management

3 March 2025,

Schneider Electric South Africa, a leading provider of energy management and automation solutions, carries the full range of SpaceLogic Living Space Particulate Matter (PM) Series sensors, which redefine indoor air quality management.

Providing comprehensive particulate matter monitoring, these PM sensors elevate the standard for commercial buildings, not only helping to optimise energy efficiency but also safeguarding the health and well-being of occupants.

Mark Freeman, Offer Manager, Digital Building for Anglophone Africa at Schneider Electric, notes that the SpaceLogic Living Space PM sensor range is compatible with any Building Management System (BMS) and can be integrated with third-party systems via multiple

selectable outputs, namely Analogue, Protocol-BACnet and Modbus). This all-in-one sensor simplifies the process of updating existing buildings.

Comprehensive sensing solutions

“Our advanced air quality sensors are designed to provide comprehensive sensing solutions for both residential and commercial spaces, ensuring a healthier and more comfortable environment for occupants,” he says.

“These units monitor air quality parameters accurately and can detect issues early, helping to mitigate health risks. The CO2 and particulate matter (PM) indicator on our touchscreen models provide real-time visibility of air quality levels, ensuring optimal environmental conditions.”

The SpaceLogic PM Series comprises a versatile, multi-sensor platform available in both optimum and medium housing configurations. These sensors are specifically designed to enhance occupant well-being while also increasing comfort and optimising energy savings.

By employing performance analytics to optimise HVAC systems, these units significantly contribute to sustainability initiatives and efforts toward decarbonisation.

Freeman explains that the Living Space PM Series offers a versatile, multi-sensor platform that can measure particulate matter (PM2.5 and PM10), temperature, humidity, CO2 and Volatile Organic Compound (VOC) levels.

Output options

Each sensor converts a measurement into one of the following output options:

• pm output: 4-20 mA, 0 to 5 Vdc or 0 to 10 Vdc

• Protocol output: BACnet and Modbus via RS-485

“The Living Space PM Series is available in both optimum and medium ranges, based on application requirements and budget. Screwless terminal block wiring and automatic calibration significantly reduce both installation and maintenance costs. The Ready-Connect plug-and-play feature further streamlines the commissioning process, enhancing overall efficiency,” says Freeman.

“We are committed to delivering innovative solutions that enhance air quality and occupant comfort. Our Living Space PM Series sensors reflect our dedication to providing reliable and flexible sensing solutions for various applications.”

Ends.

About Schneider Electric

Schneider’s purpose is to create Impact by empowering all to make the most of our energy and resources, bridging progress and sustainability for all. At Schneider, we call this Life Is On.

Our mission is to be the trusted partner in Sustainability and Efficiency.

We are a global industrial technology leader bringing world-leading expertise in electrification, automation and digitization to smart industries, resilient infrastructure, future-proof data centers, intelligent buildings, and intuitive homes. Anchored by our deep domain expertise, we provide integrated end-to-end lifecycle AI enabled Industrial IoT solutions with connected products, automation, software and services, delivering digital twins to enable profitable growth for our customers.

We are a people company with an ecosystem of 150,000 colleagues and more than a million partners operating in over 100 countries to ensure proximity to our customers and stakeholders. We embrace diversity and inclusion in everything we do, guided by our meaningful purpose of a sustainable future for all.

www.se.com  

Adoption of Wiztrust's Blockchain Certification Platform

From 2nd October 2019, in order to secure its communication, Schneider Electric has been certifying its content on Wiztrust. You can check the authenticity on the website Wiztrust.com for corporate communications.
View press release (pdf, 185 kb) opens in new window
Share this page:

Chat

Do you have questions or need assistance? We’re here to help!
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.