The Harmony P6 industrial PC and software range has been designed to improve industrial productivity and operational efficiency. It connects Operational Technology (OT) to IIoT, providing organisations with the networking and display capabilities required to gain the most from their digital transformation efforts.
“The Harmony P6 not only includes clearly presented, real-time performance information for industrial systems but also the guidance staff need to improve performance and address problems before costly downtime occurs,” explains Sbo Chili, Industry Business: Offer Manager – IDHMI at Schneider Electric.
Key Harmony P6 differentiators include:
- Smart design and engineering – it is economical and takes less time to implement.
- Workforce empowerment – the embedded software allows for improved and modern visualisation and control.
- Cybersecurity – end-to-end security designed according to the IEC62443 Cybersecurity Standard for Control Systems.
- Features associated security software, Achilles and McAfee and EcoStruxure Secure Connect Advisor for remote connections.
“When combined with Schneider Electric’s EcoStruxure Automation Expert, the Harmony P6 also enables organisations to easily deploy the computing capabilities they require for those more calculation intensive applications,” explains Chili.
The Harmony P6 offers the following technical features:
- Versatile and open to applications running Windows software at the edge: HMI, SCADA, IIoT Edge, engineering and maintenance tools, and thin clients.
- Excellent visualisation and control with associated software enhancing the operator experience.
- Leverages crew reactivity for business maximisation with four high-performing Intel CPU cores for industry. -
- Consistent operator workstations at the edge with modularity to make Box PCs, Panel PCs, and monitors for the ergonomic environment while using the application.
- A solution guide and TVDAs (Tested Validated Documented Architectures) allow for ease-of-selection, integration, and maintenance of the software association with Harmony P6, and provide a single contact window for technical support and repair.
- Configured-To-Order, associated software is selected with the online configurator.
“We’ve certainly come a long way; today’s modern and modular communication offerings like the Harmony P6 are packed with the processing, display and computing power required to play a vital role in any industrial digital transformation strategy,” concludes Chili.
ends
For more information, go to www.se.com/za/en/.