Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Schneider Electric’s next generation TransferPacT Automatic Transfer Switching Equipment (ATSE) provides a high-speed modular design for maximum scalability and increased durability and performance

  • Schneider Electric launches its next generation TransferPacT ATSE product family with easy installation and commissioning.
  • The next generation of ATSE ensures power continuity and reliability to help maximise uptime.
  • A robust, compact design reduces panel space and ensures enhanced performance in extreme conditions.

 

Schneider Electric, the leader of digital transformation of energy management and automation, today announced the launch of its next generation TransferPacT Automatic Transfer Switching Equipment (ATSE) – a range of high speed, compact, modular intelligent automatic transfer switches that offer increased scalability and robust performance

Designed according to IEC 60947-6-1, TransferPacT is a PC class ATSE available from 32A–160A, 2,3,4 pole with a rated operating voltage of 220V–440V.

 

The TransferPacT product family comes in two different offerings: Automatic and Active Automatic. TransferPacT Automatic provides quick settings and an easily viewed interface. TransferPacT Active Automatic offers a more comprehensive functionality, with a built-in controller and display, and the option to extend to an external HMI.

 

The scalability that TransferPacT provides enables a user to extend a source changeover solution so that further transfer switch modules can be added as demand grows and upgrades can be scheduled without any interruption of power.

 

TransferPacT ATSE features include increased power availability and efficiency boosted by connectivity and cybersecurity. Uptime is maximized with innovative technology that ensures transfer speeds of < 500ms. A compact and robust design helps TransferPacT perform in the harshest environments, with operating temperatures of -25°C through to 70°C. A built-in DPS and sensing wire means users enjoy a 30% time saving on installation and commissioning.

EcoStruxure IoT-enabled solutions collects and analyses ATSE data in real-time via wireless connectivity giving operators proactive – rather than preventive – maintenance analysis.

Given its robust and reliable performance that maintains power continuity and sustainability, TransferPacT ATSE has been specifically designed to boost the buildings sector, healthcare facilities, data centres, and transportation.

With the next generation TransferPacT ATSE product family, Schneider Electric further establishes its dedication to maximising uptime and enhancing safety, reliability, and connectivity for industry professionals.

 

Adoption of Wiztopic's Blockchain Certification Platform

From 2nd October 2019, in order to secure its communication, Schneider Electric has been certifying its content on Wiztrust. You can check the authenticity on the website Wiztrust.com for corporate communications.
View press release (pdf, 185 kb) opens in new window
Share this page:

Chat

Do you have questions or need assistance? We’re here to help!