Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.

The convergence of intelligence – DCS, SCADA and TLC

By Kobus Vermeulen, Direct Sales Executive, Process Automation at Schneider Electric

17 September 2024,

 

In the early days of industrialisation, control systems were primarily mechanical and relied on manual intervention and simple feedback loops to manage processes. And whilst it sounds positively medieval compared to today’s technologies, these systems played a very important role in man and machine’s industrial evolution.

Fast forward to the middle of the 20th century and electronics and computing technologies had advanced to a point where industries could leverage automated systems that require minimal human intervention.

 

These early digital control systems were centralised, with a single controller managing multiple processes. However, they had limitations like single points of failure and scalability challenges.

Now in the 21st century, industrial process automation systems are mind-blowingly intelligent and provide almost unparalleled control and monitoring capabilities, making it integral to modern industrial systems.

 

Intelligence like no other

 

At the forefront of these intelligent systems are Distributed Control Systems (DCS), Supervisory Control and Data Acquisition (SCADA), and Total Load Control (TLC) systems which have significantly transformed the industrial automation landscape.

Each system plays a distinct yet complementary role, enhancing the efficiency and sustainability of industrial processes. DCS centrally manages complex processes while SCADA focuses on remote monitoring and control, and TLC optimises energy management by regulating electrical loads. Quite the industrial trifecta.

It is also the convergence of these three systems into unified solutions that is driving the proverbial next wave of industrial automation, marked by enhanced efficiency, resiliency, and intelligence.

 

Trifecta of intelligence

 

As mentioned, the integration of DCS, SCADA and TLC into unified systems leads to fundamental benefits such as:

  • Streamlining operations - unified systems consolidate various control functions, reducing complexity and improving overall efficiency. By integrating different automation and control layers into a cohesive platform, businesses can eliminate redundancy, simplify maintenance, and enhance system interoperability.
  • Comprehensive data utilisation which leverages data synergies across different streams, enabling more comprehensive monitoring, control, and analysis. This complete view provides operators with actionable insights, supporting predictive analytics and better operational decision-making.
  • Cost-effectiveness and resource optimisation: Integration minimises redundancy, optimises resource allocation, and enhances energy efficiency, leading to more sustainable and productive outcomes. Standardised interfaces and protocols reduce the costs associated with system integration, expansion, and maintenance.
  •  

From the above it is clear that the integration of DCS, SCADA, and TLC systems empowers companies to make data-driven decisions whilst optimising operations. Plus, if one adds AI analytics and IoT into the mix these systems become even more optimised:

  • AI enables real-time data processing and pattern recognition, allowing quick responses to changes and anomalies.
  • AI predicts equipment failures by analysing sensor data, reducing downtime through proactive maintenance.
  • AI and IoT drive systems towards autonomous control, enhancing efficiency and reducing human intervention.
  • AI dynamically adjusts parameters for optimal performance and energy efficiency.
  • AI and IoT process data at the network edge, minimizing latency for faster responses.

 

Ultimately, the industrial automation marketplace is set to become even more intelligent, providing fundamental benefits to organisations and industry alike. In fact, at the current growth rate, in the next few years, today’s systems might even sound slightly outdated.

Adoption of Wiztopic's Blockchain Certification Platform

From 2nd October 2019, in order to secure its communication, Schneider Electric has been certifying its content on Wiztrust. You can check the authenticity on the website Wiztrust.com for corporate communications.
View press release (pdf, 185 kb) opens in new window
Share this page:

Chat

Do you have questions or need assistance? We’re here to help!
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.