Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

The industrial era of wireless telemetry and radio communication

By Kobus Vermeulen, Direct Sales Executive, Process Automation at Schneider Electric

21 October 2024,

 

Worldwide, there has been a concerted effort to phase out older network technologies like 2G and 3G. The radio spectrum is finite, and whilst difficult to imagine, these older mobile technologies are literally taking up valuable space.

To place it into perspective, groundbreaking for its day, 2G and its subsequent standards GPRS and EDGE are almost obsolete; offering downloads speeds of a mere 114 Kbps which is eye wateringly slower than today’s 5G connections.

For some, it might feel that we are arranging a radio spectrum funeral, but it’s good news. In its place, 4G and 5G are offering blistering speeds of up to between 10 and 20 Gbps, and moreover, wireless telemetry and radio communication systems are becoming major tools in today’s industrial settings.

 

Wireless telemetry and radio communication in context

 

Today’s advanced wireless telemetry offer a range of benefits that go beyond cost savings, including greater flexibility and mobility, remote monitoring capabilities, and enhanced safety.

It also allows for real-time data transmission, which improves decision-making processes and ensures faster responses to operational changes. These features have made wireless telemetry systems a more scalable and adaptable option, further increasing its adoption in industrial settings.

 

Radio-based systems, when compared to 2G, support enhanced data rates, offering faster and more efficient communication. Additionally, radio-based systems provide improved coverage, especially in challenging environments, where the reliability of connectivity is critical for smooth operations.

The interoperability of modern radio systems - with various devices and protocols - also makes it compelling choice for industrial operators looking to future-proof their communication networks.

 

The transition to radio telemetry

 

The move to radio-based telemetry, however, presents its own set of challenges. Infrastructure redesigns are often required to facilitate line-of-sight communication, which may involve significant reconfiguration of network layouts and installation of new radio masts.

This process therefore requires careful planning to address potential interference and ensure comprehensive signal coverage across industrial facilities.

 

However, and conversely, the transition offers exciting opportunities; industrial operators can leverage the flexibility of radio systems to design tailored solutions that meet specific requirements.

Furthermore, the deployment of new radio infrastructure allows for scalability, accommodating future expansion while also integrating advanced features like mesh networking and improved data rates.

 

4G and LTE in industrial settings

 

The adoption of LTE and 4G networks in industrial communication is expected to deliver significant benefits, particularly in terms of operational efficiency.

High-speed data transfer and improved bandwidth enable real-time transmission of large volumes of data, enhancing monitoring capabilities and supporting time-sensitive applications. The reliability and scalability offered by these advanced networks ensure that industrial systems remain adaptable to future demands, reducing downtime and operational disruptions.

Moreover, LTE and 4G networks facilitate remote access and control, allowing industrial operators to manage equipment and processes from off-site locations. This reduces the need for on-site monitoring and maintenance, which is not only cost-effective but also improves overall operational flexibility.

 

Real-world solutions

 

Schneider Electric’s Datalog A-4G Datalogger has been designed to overcome the limitations of outdated bandwidths, providing a robust solution for modern industrial communication needs.

The Datalog A-4G offers higher data transfer speeds, remote monitoring capabilities, and advanced security features, all of which are essential for ensuring the reliable and secure operation of industrial systems.

 

Looking at Schneider Electric’s telemetry solutions, these include Foxboro SCADA RTUs (remote terminal units) which been designed for efficient, cost-effective process automation. Its modular construction and advanced features make configuration and operation reliable, even in demanding applications.

Schneider Electric’s Triodata radios come in both licensed and license-free wireless solutions for SCADA and remote telemetry applications. And lastly is EcoStruxure Geo SCADA Expert, which has been optimised for managing remote assets spread across geographically dispersed infrastructure.

Adoption of Wiztopic's Blockchain Certification Platform

From 2nd October 2019, in order to secure its communication, Schneider Electric has been certifying its content on Wiztrust. You can check the authenticity on the website Wiztrust.com for corporate communications.
View press release (pdf, 185 kb) opens in new window
Share this page:

Chat

Do you have questions or need assistance? We’re here to help!