{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Setting up the reference template on the ATV320 drive for pedestal mode?
Issue:
Setting up the reference template on the ATV320 drive for pedestal mode.

Product Line:
ATV32 and ATV320

Environment:
All

Cause:
Customer wants to have his 4-20mA reference signal follow 0 to 60hz even with a low speed setting on the drive of 10hz.

Resolution:
To adjust your speed reference for a 0-100% reference for 0-60hz please adjust the following.
CONF, FULL, I/O menu, BSP
Change to bLS= Pedestal mode.
This will allow 0 speed to be 0 reference instead of using LSP as 0 reference.

Schneider Electric South Africa