Schneider Electric Gulf Countries and Pakistan Website
Welcome to our website.
Virtualization & Thin Clients
Whether you are starting up a new facility or seeking to maximize return on existing assets, server virtualization is a new option worthy of consideration.
Experience true operational agility and production schedule integrity throughout your system’s lifecycle with EcoStruxure™ Foxboro DCS virtualization technology.
From the start, the ability to host multiple virtual machines on a single control processor can significantly reduce the risk associated with project delivery cycles.
Virtualization decouples system hardware from system design, and from the geographic locations of engineering experts. Last-minute changes become much easier to implement. Virtualization technology also means software and operating systems need not be tied to specific hardware. So as your system evolves, maintenance needs and troubleshooting can be quickly addressed by Schneider Electric experts within the virtual environment.
Features
Virtualization server host with high-end processor speed, up to 96 GB of memory, up to eight internal redundant array of independent disk (RAID) systems with hot-swap drive and redundant hot-swap power supplies
Capability to host multiple virtual machines running Microsoft Windows Server® 2008 R2 Standard operating system
Support of hypervisor technology with Microsoft® Hyper-V™ Manager