{}

Onze merken

Impact-Company-Logo-English Black-01-177x54

Welkom op de website van Schneider Electric

Welkom op onze website.
Populaire vragen (FAQ's) zoeken
What is the part number for the disconnect handle on the S-FLEX SFD212 enclosed unit?
Issue:
Disconnect handle part number for S-Flex 212 enclosed unit.

Product line:
S-Flex

Environment:
All models, all serial numbers

Cause:
The exterior handle for the disconnect needs to be replaced.

Resolution:

There are 2 different handles used over the years, so please review the attachment for photos to verify which is needed:
Older drive cabinets use handle part number is 9421LH3.
Newer drives use GS2AH130

Schneider Electric Belgium

bijlage(n)
S-Flex disconnect handle.docx [86.01 KB]
Ontdek meer
Productfamilie
Mogelijk nuttige artikelen
Ontdek meer
Productfamilie