Issue:
How to calculate the heat dissipation in BTU per hour
Product Line:
All Schneider product lines
Cause:
The calculation to determine the BTU for adding a piece of equipment to a cabinet to prevent overheating.
Resolution:
To calculate heat dissipation, multiply watts by 3.4192. The result will be expressed as 1 kW is equal to BTU / HR.
פורסם עבור: שניידר אלקטריק ישראל