To activate or deactivate the Front USB port on the HMIDT732 panel when connected to a HMIG5U, goto the Windows Start Menu and launch the application Front USB Setting. The application will provide two options, enable or disable. Once a setting change has been made, the HMIG5U will reboot.
게시 대상:슈나이더 일렉트릭 Korea