FAQ 검색
What do we have to choose between low and high concerning the alarms ?
If a "Normally Closed" output must be connected to the alarm input then choose Low state as the active state. If a "Normaly Open" output must be connected to the alarm input then choose High state as the active state.