What is the U-height of the upper and lower ducts on AR7715?
Issue:
Customers want to know overall height of the AR7715, plus the equipment they're installing into it.

Product Line:
AR7715

Environment:
All versions and serial ranges.

Cause:
A customer needs to determine how much U-space the side airflow duct kit uses, so they know how much available space that leaves in the caibnet.

Resolution:

The ducts of the AR7715 take 2U each, for a total of 4U. Adding 4U to the height of the switch installed inside the AR7715 gives the total U-height.

Schneider Electric Norway

Finn ut mer
Rekkevidde:
Artikler som kan være nyttige
Finn ut mer
Rekkevidde: