Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Schneider Electric Simplifies Switchboard Installations with Resi9 RCBO + MaxBar Solution

New Zealand

15/05/2024

Schneider Electric is simplifying residential switchboard installations with the innovative MAXBAR and RCBO system, making installations up to two times faster than traditional methods. The new Resi9 range offers faster installation, space savings, and larger terminal sizes, providing significant benefits to electricians and homeowners alike.

Six months after the successful launch of its innovative next-generation residential circuit protection range Resi9™, Schneider Electric, a global specialist in energy management, is embarking on a mission to simplify residential switchboard installations by promoting benefits of best in-class MAXBAR and RCBO system. The shift from RCD/MCB to Slim RCBO with the innovative new MAXBAR™ makes installations faster and neater.

The MAXBAR is a busbar that delivers phase and neutral supply to all Resi9 RCBOs and AFDDs while connecting directly to the main switch. This makes installation up to two times faster than the traditional MCB+RCCB method.

Ray Dunn, NZ Country President at Schneider Electric, says, “Resi9 is at the forefront of global technology with the advent of MAXBAR and RCBO, which offer significant benefits and advantages to electricians seeking to grow their business. At Schneider Electric we understand that electricians are not just looking for the next generation of circuit protection – they want to differentiate their own businesses through innovation and efficiencies, such as less nuisance tripping and less inconvenience when an earth leakage is detected, which please their customers.

We understand that RCBOs are more expensive than MCB/RCD devices, but when you price RCBOs in a complete installation and factor in labour savings, material, and enclosure, the overall install cost is a lot closer. Because of the space savings in a board redesign using Resi9 devices, the cost of adding RCBOs could be more than offset by not having to replace a full board. Slim RCBOs are perfect for renovations which may include adding additional circuits such as EV charging, heat pumps, or induction cook tops.

“RCBO is the future of switchboard protection, and the time-saving benefits of the Slim RCBO and MAXBAR solution enables electricians to streamline their day, serve their customers and ensure their satisfaction, and spend more time on everything else that matters to them.”

Electrician Sarah Kirk says, “I found the new MAXBAR method considerably quicker to fit off compared to the normal RCCB/MCB method. It also took up a lot less room in the switchboard, meaning more space for any future or additional work done.

“I was pretty stoked with the functionality of the new Resi9 switchgear, which is also clean, sustainable, and super-easy and quick to install, which makes a big impact on your day-to-day work as an electrician. The larger terminal sizes were a big thumbs-up from me, much easier to double up those larger cables.”

The Resi9 range launched last October and has replaced the previous range, Domae, which was discontinued at the end of February 2024.

Resi9 key product features:

  • Up to 2 times faster installation speed with MAXBAR compared to the RCCB/MCB installation.
  • No cables needed for feeding RCBOS with MAXBAR connecting main switch directly to any type of Resi9 RCBO and AFDDs.
  • Opportunity to grow business with latest innovation in circuit protection – AFDD.
  • Simplify communication with homeowners using easy to explain pictograms on all devices.
  • All the product-related information (specifications, brochures, catalogues, FAQs and installation instructions) at your fingertips by scanning the QR code on all products.

Adoption of Wiztopic's Blockchain Certification Platform

From 2nd October 2019, in order to secure its communication, Schneider Electric has been certifying its content on Wiztrust. You can check the authenticity on the website Wiztrust.com for corporate communications.
View press release (pdf, 185 kb) opens in new Window
Share this page:

Chat

Do you have questions or need assistance? We’re here to help!