The Altivar Process drive systems configurator tool is a valuable resource for configuring variable-speed drives, such as the ATV660, ATV680, ATV960, and ATV980 drive ranges. It's a part of our configured drive system approach, enabling users to easily customise their enclosed drives to meet specific application needs. The tool simplifies the selection of the appropriate speed drive systems and accessories, ensuring compatibility and optimal performance.
Configure your individual Altivar Process drive system
Configure your individual drive system in just a few clicks with the Altivar Process Configurator tool. Its predefined options significantly reduce delivery time for individually adapted drives, ready to connect.