Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
What does LSIG signify on Micrologic trip units?

Issue: What are the LSIG trip unit functions on a Micrologic trip unit? Product Line: Circuit Breakers Resolution: The letters LSIG signify the type of protection and available adjustments on certain...

What is the difference between sub feed lugs, through feed lugs, and sub...

Issue: What is the difference between sub-feed lugs, through-feed lugs, and sub-feed breakers? Product Line: Panelboards Environment: Applies to NQ and NF Panelboards Resolution: Sub feed lugs are a...

Download links for Vijeo Designer 6.2 SP12

Issue: Where can we find the download links for Vijeo Designer V6.2 SP12? Product Line: Vijeo Designer V6.2 (all hotfixes and service pack revisions less than SP12) Resolution: Please find the...

Per the NEC, what are the standard ampere ratings of fixed-trip circuit...

Issue: Where do circuit breaker amp ratings come from? Product Line: Circuit Breakers Resolution: Per NEC 240.6, the standard ampere rating for inverse time, fixed-trip circuit breakers, 600Vac...

What sets Type 1 and Type 2 Surge Protective Devices (SPD) apart from each...

Issue : What sets Type 1 and Type 2 Surge Protective Devices (SPD) apart from each other? Product Line: TVSS/SPD Environment: Application Cause: Clarification Resolution: ​​​​​​​Type 1: These are...

What are the standard single phase and three phase kVA ratings for...

Issue: Listing of standard Transformer kVA sizes Product Line: LV Transformers Environment: Applies to Low Voltage Transformers by SquareD/Schneider Electric Cause: Transformer kVA levels fall into...

How to Calculate the Required Capacity kVA Rating or Amperage Capacity for...

Issue: Calculation of kVA capacity for a Single or Three Phase Transformer, based on Winding Voltage and Amperage information. Product Line: Low Voltage (LV) Transformers Learn more about DOE 2016...

How hot can circuit breakers get? What is the temperature of a molded...

Issue: What is the temperature of a molded case breaker? Product Line: Circuit Breakers Resolution: See data bulletin 2700DB9901 for detailed information regarding the circuit breaker operating...

Show more
Popular Video FAQsPopular Videos
Show more
Learn more through our General Knowledge FAQsGeneral Knowledge
How to load an M172 project with a USB memory stick

The power to the M172 should be turned off ( no connections to the USB mini port for programming ) Then insert the USB stick and then apply power. At boot-up the M172 will detect the USB memory stick...

What is the difference between PNP and NPN when describing 3 wire...

Most industrial proximity sensors (inductive, capacitive, ultrasonic and photo electric) are solid state. The term solid state refers to the type of components used within the sensor. Solid state...

What is the difference between in-sync and in-phase?

There is often confusion between the in-phase and the In-sync features of ASCO transfer switches. It is important to understand the difference between these features especially during the process of...

How do I become a supplier for Schneider Electric?

Issue: How to become a supplier for Schneider Electric Product Line: Source Materials Environment: Products sold and used in the United States Resolution: For information and help on becoming a...

What do the terms AC1 and AC3 mean?

Issue: What are the utilization categories AC-1 and AC-3? Product Line: Schneider Electric Products Environment: Inductive and Resistive Loads Resolution: AC-1 - This category applies to all AC loads...

How to have access to M218 controllers in Machine Expert

NOTE: M218 are obsolete controllers, from v2.2 they stopped being integrated into Machine Expert. Machine Expert v2.1 or below is needed for the Local Offer Code to work The M218 controllers are not...

Insulation Resistance Testing and Humidity

Issue: How does humidity affect insulation resistance testing results? Product Line: Circuit Breakers Environment: Molded case and insulated case breakers Resolution: High humidity can drastically...

What does the term "NEMA Type 1A" refer to?

NEMA Standards Publication 250-1997, "Enclosures for Electrical Equipment (1000 Volts Maximum)" no longer lists this enclosure type. This enclosure type is commonly accepted to be referring...

Show more
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings