Search FAQs

What is the expected life of my APC UPS VRLA battery?

Article available in these languages:

  • Spanish
  • , French

Issue:
What is the expected life of my APC UPS VRLA Battery?

Product Line:
All UPS Models

Environment:
All Three Phase and Single Phase UPS Models

Cause / Resolution:
Most APC batteries should last three to five years. There are many factors which affect Battery life including environment and number of discharges. Below are some guidelines to ensure optimum life expectancy:


1. Operating Temperature:

The optimal operating temperature for a lead‑acid battery is 20–25°C (68–77°F). Operating at higher temperatures significantly reduces battery lifespan. As a general rule, every 8°C (15°F) increase in temperature will cut the battery’s life in half.

For example, a battery expected to last 4 years at 25°C (77°F) would only last about 2 years if operated at 33°C (95°F).

Keep in mind that the internal battery temperature of a UPS is always higher than the ambient room temperature. Because of this, it is strongly recommended to install the UPS in a location with good airflow, proper ventilation, and adequate cooling to help maximize battery life.


2. Battery Calibration and Deep Discharge:

You should perform runtime calibrations on your UPS only once or twice per year, and only if truly necessary. While some customers run calibrations to verify that their available runtime is sufficient, performing these tests too frequently can significantly shorten the lifespan of the APC battery.

It is also important to remember that a UPS is not designed for frequent deep‑discharge cycles. We do not recommend using an APC Smart‑UPS or Back‑UPS as a portable power source that is repeatedly discharged and recharged (for example, when mounted on a mobile equipment cart). These units are specifically engineered for emergency backup power during unexpected outages or brief power interruptions—not for continuous cycling like a portable battery pack.



3. Storage:

APC batteries should not be stored for extended periods of time. New batteries or UPS units should be stored for no longer than 6 months from the date of purchase, as they leave the factory at approximately 80% charge. After this period, the battery should be placed into use; otherwise, it will lose a significant portion of its charge.

It is also not recommended to store batteries that have already been in use. Long‑term storage without periodic recharging can lead to reduced lifespan and unpredictable performance.

Temperature and Storage Recommendations

Storage temperature has a major impact on how quickly a battery degrades while not in use:

  • –15°C to +30°C (5°F to 86°F):
    Perform a full recharge cycle at least every 6 months.

  • +30°C to +45°C (86°F to 113°F):
    Perform a full recharge cycle at least every 3 months.

Proper storage temperature and periodic recharging are essential to preserving battery health and ensuring reliable performance when the UPS is finally placed into service.


4. Load:

As the load on your UPS increases, the available runtime decreases. For best performance and battery longevity, it is recommended not to exceed 80% of the UPS’s rated capacity.

If a power outage occurs while the UPS is operating at or near full load, the battery will discharge much more quickly, reducing the amount of backup time available. Frequent heavy loads and rapid discharges can also significantly shorten the battery’s overall life expectancy.


5. Battery chemical reaction:

As a VRLA (AGM) battery ages, it undergoes a chemical process known as sulfation. This occurs when lead sulfate crystals harden on the battery plates, reducing the battery’s ability to charge and discharge efficiently.

This can lead to several noticeable effects:

  • Longer charging times than normal
  • Excessive heat buildup, which can eventually cause electrolyte “boil‑out”
  • Shorter runtimes between charges
  • Significantly reduced overall battery life

6. Battery replacement:

Since the typical end‑of‑life for VRLA batteries is approximately five (5) years, it is strongly recommended to replace the UPS battery before reaching this age. Doing so helps prevent performance degradation and reduces the risk of possible hydrogen sulfide gas emission, which can occur when aging batteries begin to fail.


7. Firmware Improvements:

For selected single‑phase Smart‑UPS models, it is recommended to update the UPS firmware to the latest available version. This ensures the unit benefits from all battery‑related enhancements, stability improvements, and performance optimizations provided by APC.

For instructions and compatibility details, refer to FA164737, which outlines the process for updating firmware on supported single‑phase Smart‑UPS units.

If you have any clarifications, please feel free to contact us at 1-800-800-4272 or chat with our technical support representatives.

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Our Mission
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Financial Results
  • Annual Reports
  • Share Price
  • Investor Events
  • Sustainability
  • New Energy Landscape
  • Next-generation Automation
  • AI and Technology
  • Reports
  • Foundation
  • Consulting
  • Help Center
  • Solutions
  • Software
  • Blog
  • General Terms of Business
  • Global - FR
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Change your cookie settings