Search FAQs
Video: How does one set up the ATV61/71 keypad VW3A1101 to display more than one parameter?
Issue:
ATV61/71 keypad VW3A1101 set up to display more than one parameter.
Product line:
Altivar 61 and 71
Environment:
All models, all serial numbers:
Cause:
One parameter is the default.
Resolution:
From the main menu go to menu 6 [Monitoring Config] then enter
Select 6.2 [MONITOR SCREEN TYPE].
If "Digital value type" is "Digital" only two parameters can be selected.
If "Digital value type" is "Bar graph" only two parameters can be selected.
If "Digital value type" is "List" then five parameters can be selected.
Go to "PARAMETER SELECTION". Select the check box beside the parameters you want to display.
ATV61/71 keypad VW3A1101 set up to display more than one parameter.
Product line:
Altivar 61 and 71
Environment:
All models, all serial numbers:
Cause:
One parameter is the default.
Resolution:
From the main menu go to menu 6 [Monitoring Config] then enter
Select 6.2 [MONITOR SCREEN TYPE].
If "Digital value type" is "Digital" only two parameters can be selected.
If "Digital value type" is "Bar graph" only two parameters can be selected.
If "Digital value type" is "List" then five parameters can be selected.
Go to "PARAMETER SELECTION". Select the check box beside the parameters you want to display.
Released for:Schneider Electric Global
Explore more
Explore more