Unity Pro error message 'Project is read only'.
Issue:
Error message is displayed when trying to open a Unity Pro project.
Product Line:
Unity Pro programming software
Resolution:
- Is the project open in another session of Unity?
- Go to the Windows Explorer. Right click on the project file and verify that the 'read only ‘ attribute is not set.
- Is the Unityxl.ini file attribute set for ‘read only’?
- Go to Tools – Options – Connection. Make sure that programming mode is set.
- File - Open. Make sure that 'read only mode' is not checked in the 'Open Options' in the lower left corner of the Open box.
If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance: