Search FAQs

What is the maximum torque rating for the ATV630?

Issue:
Torque rating for the ATV630

Product Line:
ATV630

Environment:
All models and serial numbers

Cause:
None

Resolution:
110% of maximum continuous current for 60 secs for ATV600, with Dual Rating (5.2 menu)=Normal rating , 120% of maximum continuous current for 60 secs for ATV900 with Dual Rating=Normal rating.
150% of maximum continuous current for 60 secs for ATV 630 and ATV 930, with Dual Rating set to Heavy Duty.

The maximum torque of the drive, the more current we have, the more torque we have, but for this depends on :
For asynchronous motors: the torque performance is linked to the efficiency of the motor.
On permanent magnet motors: there is no over torque capability, 120% of over current will reach 120% of over torque (1.2).

For example with ATV71, its 165 % of over current we can reach 2.2 . Then with 120% of overcurrent we can reach 1.6  (but not with all motors).

Schneider Electric Global

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Our Mission
  • Company Profile
  • Report a misconduct
  • Accessibility
  • Newsroom
  • Financial Results
  • Annual Reports
  • Share Price
  • Investor Events
  • Sustainability
  • Electricity 4.0
  • Next-generation Automation
  • AI and Technology
  • Reports
  • Foundation
  • Consulting
  • Global - FR
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Change your cookie settings