It is not possible to replace the cables, The cables are not detachable from the motor body. They are part of the motor. Their length is 400mm, see attached pages.
פורסם עבור:שניידר אלקטריק ישראל


{}
It is not possible to replace the cables, The cables are not detachable from the motor body. They are part of the motor. Their length is 400mm, see attached pages.