Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
We offer a full range of Testing & Certification to customers with respect to Indian & International standards and is accredited by NABL as per ISO/IEC17025 : 2017.

We serve all customers in testing of all types of electrical products that help meet both National and International standard requirements.

The main motto of the GIGA labs is the highest customers satisfaction, impartiality & confidentiality of the tests.The management ensures to be the best-in-class in technical expertise, innovation,and technology used for test methods and processes.
  • One of Schneider Electric’s 5 Global labs which is spread across 5300 sq.mts.
  • Accredited by NABL & Compliant as per ISO/IEC 17025:2017.
  • Equipped with Electro-Mechanical, Electronics, Automation, and in-house prototyping capabilities.
  • Follows stringent quality process and develop technical expertise to strive for “Best in Class”.

Key Differentiators

Temperature controlled - Walk-in chamber

Dimension : L 6m X W 4 m X H 3.2 m
One of a kind in India, this walk-in chamber controls the temperature from 0 to 70°C with the temperature rise test facility up to 6KA.

Inhouse Prototyping workshop

Fully equipped prototyping workshop for fixtures and other requirements

Digital service for testing services

With IP camera, it is possible for the client to witness the live test remotely from anywhere in the Schneider Electric network.
priority slot booking

Priority slots

We understand business priorities ! Reserve the priority slots for business continuity .

Comprehensive Testing Lab

A One-stop solution for pre-compliance, and compliance testing, and regulatory certification with complete confidentiality of tests.

More than 10 years of Experiences in Electrical Product Testing covering Low Voltage tests , Functional tests, Environmental tests, and EMC tests
A person using mobile phone in Electric office

Speed

We follow global test methods and have a deeper understanding of products and standards to provide accurate & faster test results. On-time completion with the highest quality of testing.

A recognized and accredited laboratory

GIGA Labs is ASTA RTL for standards including

  • Low Voltage Switchgear and Controlgear assemblies : IEC 61439-2
  • Distribution boards : IEC 61439-3
  • Busbar trunking (IEC61439-6)
  • Busbar trunking systems : IEC 61439-6
  • Switches and Socket-outlets : BS EN 60669-1, BS 1363-2, SASO 2203, SASO 443

NABL Accredited as per ISO/IEC 17025

GIGA Labs is accredited by NABL for ISO/IEC 17025 in the field of Testing for various types of electrical, mechanical & environmental tests on products like domestic switches and sockets, LV circuit breakers, industrial switches and controlgear, LV switchgear and control gear assemblies, distribution boards, busbar trunking systems and many more.

NABL (National Accreditation Board of Testing and Calibration Laboratory) is a constituent board of Quality Council of India. It is a full member of ILAC and a MRA signatory to ILAC for accreditation program for ISO/IEC 17025.

CTF as per IECEE CB Scheme

GIGA Labs is a Customer Test Facility (CTF) according to IECEE CB Scheme for Safety Standards of IEC 61010 series. It is accredited under the UL (Demko) NCB.

For more details, visit www.iecee.org

Download GIGA Lab Brochure

Click Here
Closeup shot of hand shake by two men

Contact us

GIGA Labs Located at Whitefield, Bangalore
Click Here

Need help?

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Start your sales enquiry online and an expert will connect with you.

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Centre

Find support resources for all your needs, in one place.

Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.