Sök bland vanliga frågor (FAQ)
The Compact NSXm160 is compatible with installation on DIN rails in Prisma G and P enclosures?
The NSXm160 is compatible with DIN rail installation in Prisma P and G switchboards.
The installation can be made on adjustable DIN rails with reference numbers 03402 (Prisma P) or 03002 (Prisma G).
The installation can be made on adjustable DIN rails with reference numbers 03402 (Prisma P) or 03002 (Prisma G).
Publicerad för:Schneider Electric Sverige
Utforska mer
Produktfamilj
Utforska mer
Produktfamilj