How do I access the Com Scanner Input and Output tables on the Altivar Process Drive?

Article available in these languages: Finnish

Issue:
Access the Comm Scanner Input and Output tables on the Altivar Process Drive.

Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)

Environment:
All serial numbers for Altivar Process Drive

Cause:
To configure the Comm. Scanner (Input/Output) tables:

Resolution:
Programming from the Drive:
  • [Communication] [Comm parameters] [Modbus SL] [Modbus Fieldbus] [Com. scanner input]
    • Up to 8 input registers can be configured
    • By default the first 2 registers are pre-configured
      • [Scan. IN1 address] nMA1 - 3201 (EtA Status word)
      • [Scan. IN2 address] nMA2 - 8604 (rFrd - Output frequency)
  • [Communication] [Comm parameters] [Modbus SL] [Modbus Fieldbus] [Com. scanner output]
    • Up to 8 output registers can be configured
    • By default the first 2 registers are pre-configured
      • [Scan.Out1 address] nCA1 - 8501(CMd word)
      • [Scan.Out2 address] nCA2 - 8602(LFrd - Output freq in rpm)



Programming from Somove:
  • [Parameter List] [Fieldbus] [Port - Modbus Serial] [Modbus Fieldbus]
screenshot

NOTE: This is not the same as the I/O scanning table that is used with Ethernet communications.


Schneider Electric Україна

Досліджуйте більше
Серія:
Статті, які можуть бути корисними
Досліджуйте більше
Серія: